To set up a
PUCCH for an Advanced LTE-A FDD Uplink carrier, click the Wizard button
in the Uplink node to open the PUCCH Configuration Wizard.
The wizard supports 3GPP technical specification 36.141.
In multi user PUCCH test, four signals are configured: one wanted signal and three interferers, which are transmitted via separate fading paths using relative power settings shown in Annex A.9.
When the uplink is configured with four antennas, the PUCCH Wizard button is not enabled.
|
PUCCH Test Configuration (dNB Performance Test based on 36.141) |
36.141-8.3.3: Tested Signal |
36.141-8.3.4 ACK missed detection for PUCCH format 1b with Channel Selection |
|---|---|---|
|
RS Orthogonal Cover / ACK/NACK Orthogonal Cover
|
Single Antenna Configuration
Choice:
36.141-8.3.3 ACK missed detection for multi user PUCCH format 1a
36.141-8.3.4 ACK missed detection for PUCCH format 1b with Channel Selection
36.141-8.3.5 ACK missed detection for PUCCH format 3
36.141-8.3.9 CQI performance requirements for PUCCH format 2 with DTX detection
Default: 36.141-8.3.3 ACK missed detection for multi user PUCCH format 1a
Two Antenna Configuration
Choice:
36.141-8.3.7 ACK missed detection for PUCCH format 1a transmission on two antenna ports
36.141-8.3.8 CQI performance requirements for PUCCH format 2 transmission on two antenna
36.141-8.3.9 CQI performance requirements for PUCCH format 2 with DTX detection
Default: 36.141-8.3.7 ACK missed detection for PUCCH format 1a transmission on two antenna ports
For Both Antenna Configurations:
Double-click or use the drop-down menu to set the PUCCH Test Configuration Type.
The choice and default value depend on radio format and antenna configuration.
When the uplink is configured with four antennas, the PUCCH Wizard button is not enabled.
When the PUCCH Test Config Type is 36.141-8.3.8 or 36.141-8.3.9, this read only parameter is displayed.
Choice: Tested Signal | Interferer #1 | Interferer #2 | Interferer #3
Default: Tested Signal
Double-click or use the drop-down menu to set the Signal/Interferer Type.
This parameter is shown when single antenna configuration and PUCCH Test Configuration Type is 36.141-8.3.3. Otherwise it is hidden.
Range: Random HARQ-ACK Length 4AN
Default: 4AN
Displays the Random HARQ-ACK Length as 4bits (4AN), when the PUCCH Test Configuration Type is 36.141-8.3.5. Otherwise it is hidden.
See 3GPP TS 36.141 for more information.
This parameter is available only when PUCCH Test Config Type = 36.141-8.3.5 ACK missed detection for PUCCH format 3.
Double-click or use the drop-down menu to set the system bandwidth and number of resource blocks.
This parameter choice is limited by 10/15/20 MHz system bandwidth when PUCCH Test Configuration Type is 36.141-8.3.4 or 8.3.5. Otherwise there is no limitation.
Default: 1a
This parameter is automatically set by the software and is not editable.
Displays the PUCCH format that is defined for each PUCCH Test Configuration Type as followings:
36.141-8.3.3 = 1a
36.141-8.3.4 = 1b
36.141-8.3.5 = 3
36.141-8.3.7 = 1a
36.141-8.3.8 = 2
36.141-8.3.9 = 2
See 3GPP TS 36.211 and 36.141 for more information.
Displays the Cell_ID that is defined for each PUCCH Test Configuration Type as followings:
36.141-8.3.3 = 150
36.141-8.3.7 = 150
36.141-8.3.8 = 150
36.141-8.3.9 = 150
Otherwise the value is editable as followings:
Range: 0 to 503
Cell ID = [(3 x Physical Cell ID Group) + Physical Cell ID Sector]
See 3GPP TS 36.211 and 36.141 for more information.
Range: 0 to 7 (36.141-8.3.4 test case)
Default: 0
Displays the N_CS(1) value that is defined for each PUCCH Test Configuration Type as followings:
36.141-8.3.3 = 0
36.141-8.3.7 = 0
36.141-8.3.8 = 0
36.141-8.3.9 = 0
Otherwise it is hidden.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 1 to 3 (36.141-8.3.4 test case)
Default: 2
Displays the Delta Shift PUCCH value that is defined for each PUCCH Test Configuration Type as followings:
36.141-8.3.3 = 2
36.141-8.3.7 = 2
36.141-8.3.8 = 2
36.141-8.3.9 = 2
Otherwise it is hidden.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 0 to Calculated Maximum Value
Dependent on related PUCCH settings.
When the PUCCH Test Configuration Type is 36.141-8.3.4, sets the n(1)PUCCH,1 value .
Otherwise it is hidden.
See 3GPP TS 36.211, 36.213 and 36.141 for more information.
When the PUCCH Test Configuration Type is 36.141-8.3.3, displays the nPUCCH(1,0) value which is determined by Signal/Interferer Type.
When the PUCCH Test Configuration Type is 36.141-8.3.7, displays the nPUCCH(1,0) value as 1.
Otherwise it is hidden.
nPUCCH(1,0): resource index of PUCCH formats 1/1a/1b for antenna port index 0.
See 3GPP TS 36.211 and 36.141 for more information.
When the PUCCH Test Configuration Type is 36.141-8.3.7, displays the nPUCCH(1,1) as 2.
Otherwise it is hidden.
nPUCCH(1,1): resource index of PUCCH formats 1/1a/1b for antenna port index 1.
See 3GPP TS 36.211 and 36.141 for more information.
When the PUCCH Test Configuration Type is 36.141-8.3.8 or 36.141-8.3.9, this displays the nPUCCH(2,0) as 1 .
Otherwise it is hidden.
nPUCCH(2,0): resource index of PUCCH formats 2/2a/2b for antenna port index 0.
See 3GPP TS 36.211 and 36.141 for more information.
When the PUCCH Test Configuration Type is 36.141-8.3.8 or 36.141-8.3.9, this displays the nPUCCH(2,1) as 2.
Otherwise it is hidden.
nPUCCH(2,1): resource index of PUCCH formats 2/2a/2b for antenna port index 1.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 0 to (Number of RB in the system bandwidth) * 5 – 1
Default: 0
When the PUCCH Test Configuration Type is 36.141-8.3.5, enables you to set the nPUCCH(3, 0) value.
Otherwise it is hidden.
nPUCCH(3,0): resource index of PUCCH formats 3 for antenna port index 0.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 1 to (Maximum resource blocks -1)
Default: 1
When the PUCCH Test Configuration Type is 36.141-8.3.8 or 36.141-8.3.9, enter the number of resource blocks per slot that are available for PUCCH Format 2/2a/2b transmissions in each slot.
In this case the minimum value is 1 to enable conformance test signal according with standard.
Otherwise it’s hidden.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 0 to max resource elements – 1.
Default: Tested Signal: 4
When the PUCCH Test Configuration Type is 36.141-8.3.3, displays the Cyclic Shift Index that is defined for each Signal/Interferer Type as followings.
Tested Signal = 4
Interferer #1 = 2
Interferer #2 = 3
Interferer #3 = 4
Otherwise it is hidden.
This parameter is automatically set by the software and is not editable.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 0 to 2.
Default: Tested Signal: 0
When the PUCCH Test Configuration Type is 36.141-8.3.3, displays the Orthogonal Cover Index that is defined for each Signal/Interferer Type as followings:
Tested Signal = 0
Interferer #1 = 0
Interferer #2 = 1
Interferer #3 = 2
Otherwise it is hidden.
This parameter is automatically set by the software and is not editable.
See 3GPP TS 36.211 and 36.141 for more information.
Range: 0 to 17.
Default: Tested Signal: 2
When the PUCCH Test Configuration Type is 36.141-8.3.3, displays the RS Orthogonal Cover / ACK/NACK Orthogonal Cover that is defined for each Signal/Interferer Type as followings.
Tested Signal = 2
Interferer #1 = 1
Interferer #2 = 7
Interferer #3 = 14
Otherwise it is hidden.
This parameter is automatically set by the software and is not editable.
See 3GPP TS 36.141 for more information.
Default: Tested Signal: 0 dB (Carrier Power = – 3 dB in the background)
When the PUCCH Test Configuration Type is 36.141-8.3.3, displays the Relative Power that is defined for each Signal/Interferer Type as followings:
Tested Signal = 0 dB (Carrier Power = – 3 dB in the background)
Interferer #1 = 0 dB (Carrier Power = – 3 dB in the background)
Interferer #2 = -3 dB (Carrier Power = – 6 dB in the background)
Interferer #3 = 3 dB (Carrier Power = 0 dB in the background)
Otherwise it is hidden.
This parameter is automatically set by the software and is not editable.
See 3GPP TS 36.141 for more information.
When the PUCCH Test Configuration Type is 36.141-8.3.3, displays the Relative Timing.
Otherwise it is hidden.
This parameter is automatically set by the software and is not editable.
See 3GPP TS 36.141 for more information.
This section provides a description for the parameters that are specific to this test type. This test configuration type provides a table that is used to select the HARQ-ACK response. For more information, refer to the 3GPP TS 36.213.
Choice: 2 | 3 | 4
Default: 4
The selection determines the number of HARQ-ACK responses and combinations (indexes).
|
PUCCH Resources (A) |
|||
|---|---|---|---|
|
2 |
3 |
4 |
|
|
Indexes |
5 |
11 |
18 |
Range: 0 to calculated maximum value that depends on related PUCCH settings
Default: 0 = 0
1 = 1
2 = 2
3 = 3
4 = 4
Set the n(1)PUCCH, n value.
Click a checkbox (check mark showing) to select an HARQ-ACK response. Clicking a new checkbox clears the previously selected checkbox. the software allows only one checkbox selection at a time. In the above figure, index 1 is checked as the response.
Displays HARQ-ACK(0) response .
Displays HARQ-ACK(1) response .
Displays HARQ-ACK(2) response . This field shows when PUCCH Resource (A) selection is 3 or 4.
Displays HARQ-ACK(2) response . This field shows when PUCCH Resource (A) selection is 4.
Displays the PUCCH resource value n(1)PUCCH.
Displays the HARQ-ACK bits.